Add the Controller

To add a controller to your project:

  • Click the New command in the File menu tso start the Controller Creation Wizard
  • Choose the motion engine option (Pipe Network or PLCopen) and select the application template (see list below)
  • Figure 5-3: Select an Application Template

  • Click the Finish button
  • Click the Save As command in the File menu
  • Define the Project Name and its Location
  • Click OK

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen